HI All
I need to develop a power supply for a thermal application. We are using a thermal peltier module. We are going to use the one that is rated to about 70W. I would like to use a PWM with a Switch mode power supply, so that I can regulate the power going to the module and adjust it depending on the required temperature and which would optimise the power consumption for when I do not need low temperatures. Can you please advise me on what devices to use and if I am correct I need to use some form of filter on the output of the power regulator before connect the Peltier?
Thank You
Regards
DJ