Hi Tiers:
Now we found a chance of AC-DC which is PSR mode in our customer which produced the PLC modem, the current solution they used is PI’s Lnk623 / Lnk625DG
and their PLC are divided by 3 specification, the standby power consumption is 0.5W and targeted is 0.3W.
Single Output |
|
Single Output |
|
Dual Output (PLC + Wifi) |
12V@0.1A and 3.3V @1.3A |
And customer want to evaluate TI's solution ,I think the proper device should be UCC28911 to them, could you please recommend a proper TI-design to their spec right now , and I can apply for one or two pcs for their evaluation as soon.
BTW, the evm of UCC28911 is 5V output so I can't use it.