Dear team.
We want to design a lead acid battery(12V) charger based on UCC28740 for output (13.5V/0.7A typ.). We want to implement a feature that whenever the battery voltage falls below 10V it should be charged at 14.4 V(boost mode) and when the voltage reaches 14.4V then charging should be at 13.5V (float mode).
We are also trying to use a MCU and power switch in the same project.
Please advise the way we can implement the same.
Regards
Rajesh Gupta