Hello,
I'm using the TPS28255 to drive a half-bridge (HB). I tie the EN pin to VCC, so it starts up at same time as VCC. When duty cycle is high (>90%), the HB intermittently gets stuck (no switching). If I disable and enable, it works fine. I found if I delay the enable signal, the TPS28255 never sees this issue.
The datasheet doesn't mention sequencing of EN pin vs VCC... in fact, the simplified schematic on page 1 shows EN pin tied to VCC. Is this an issue?
Thanks,
Zeeshawn