Hello,how is the UCC27210 behaving below UVLO (0-7V)? Are HO and LO high/low impedance? What about the range 7-8V (between VDD min and UVLO)?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,how is the UCC27210 behaving below UVLO (0-7V)? Are HO and LO high/low impedance? What about the range 7-8V (between VDD min and UVLO)?
Regards, Holger
Hi Holger,
Below UVLO, the output stage goes high impedance.
Unless, VDD reaches UVLO, the output is high impedance.
Regards,
Ritesh
Hello Ritesh,
customer has following concern: In case the boostrap voltage (Vhb-Vhs) is not high enough or not available during power up then the gate t of the HS Mosfet is not defined because the driver is high impedance. Further the LS Mosfet will switch the first time (half brigde is already under voltage) and that causes a short switching of the HS Mosfet through the Miller capacity and lead to a short of the half bridge. The available gate termination resistor of 10kohm will not help much.
This would be a big problem in LLC or primary HB applications.
To prevent this behavior customer thinks of using a clamping PNP Fet.
Regards, Holger
Hello Ritesh,
this sounds better. How is this technical realized?
You would need a gate voltage to switch on the transistors to get an low output in case of Bi-CMOS driver. In UVLO there may be no VCC and therefore the UCC27210 use hybrid driver (CMOS+BJT) or a parallel PNP switch? Please let me know how it works.
Regards, Holger