We are in the process of designing a 2KW AC/DC power supply with the following specs:
Input Voltage 85-250VAC
Output Voltage 200-350DC.
90%+ efficiency
We plan on using the UCC28180 as the first stage PFC that gives us around 400VDC. For the second stage we are looking to use the UCC28950 for isolation and for stepping-down the DC voltage to our output range. It looks like the UCC28950 can scale up to our power needs but we are suspicious if the higher output voltage is acceptable.
A few questions:
1. The design excel sheet for the UCC28950 (SLUC222C) shows a proposed power transformer turns ratio of 1. Will this work as expected?
2. Is there any concerns about running at this power level with the higher output voltage range?
3. Are there any other converters ICs that may be more appropriate for our needs?
4. We would like to control the output voltage via a microprocessor. Is there a recommended method for this?
Thank you