Hi All,
How to setting brown out. Do you have simulation tool could share to us??
Following description from datasheet page.20. Is it brown out function??
Input Under-Voltage: The line input run and stop thresholds are determined by current information at the VS pin
during the MOSFET on-time. While the VS pin is clamped close to GND during the MOSFET on-time, the current
through R S1 , out of the VS pin, is monitored to determine a sample of the bulk capacitor voltage. A wide
separation of run and stop thresholds allows clean start-up and shut-down of the power supply with the line
voltage. From the start state, the sensed VS current, I VSL , must exceed the run current threshold, I VSL(run) (typical
220 µA), within the first three cycles after switching starts as VDD reaches V VDD(on) . If it does not, then switching
stops and the UVLO reset and re-start fault cycle is initiated. Once running, I VSL must drop below the stop level,
I VSL(stop) (typically 80 µA), for three consecutive cycles to initiate the fault response.
Thanks.