Hi,
SG3524 is designed for 50kHz signal in Flyback convertor mode to generate PWM. The PINS 3(oscillator output) and 7 (CT ramp wave) are always present whethre SHDN is 0V or 1.1V.
1. Please let us know how to we confirm the controller is on or off.
Also, the Emitter output (Pin 11 $ 14) is driving the GATE of a MOSFET to run a flyback transformer. But Emitter output is not present. We are assuming as Current limitter (Pin 4) is not getting any feedback because transformer is not connected.
2. Please let us nkow how can we check for the output without connecting the transformer in the circuit to make sure GATE pulse is proper and parameters (Duty cycle) can be in our control.
For switching frequecy design, formula is given fosc = 1.3/(RT* CT)
But it is not coming practically as we have designed for fosc = 48kHz with RT = 2.7k and CT = 0.01uF