Hi!
Using the UCC25600, I'm planning to implement a LCC converter with a PFC pre-regulator and a secondary side CC control, with CV only as a OVP. The resonant tank I've designed, is supposed to operate from max to no load between 190-300KHz. Is there any extra precaution I should consider while implementing a LCC (as opposed to a LLC) with this IC. I have experience designing several LLC designs, but with NXP or ST parts. Would love to get hold of an application note specifically for LCC. Else, any user experience, extra-precautions, with respect to LCC would be very helpful.