Hi
Please help check the attached schematic.
The main trouble is when the device fails it causes a high voltage on the PWM pin which goes to the CPU and then kills the CPU.
Any comments or suggestions appreciated.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Please help check the attached schematic.
The main trouble is when the device fails it causes a high voltage on the PWM pin which goes to the CPU and then kills the CPU.
Any comments or suggestions appreciated.
Thanks
Star
Hi,
I'm sorry if continuing this here is wrong, please inform me and delete this if it is.
I've tried to just turn on this MOSFET with 5V, but i only get ~3.5V at the LED which is not enough.
I'm planing to use UCC27537 to drive the MOSFET, will it work to get full 24V to the LED?
Please help, thank you.