Hi, I tell you my problem. I'm going to use the BQ25570, it only supports a maximum of 5.1 V in Vin, and my solar panel is 6 V. I would like to limit this voltage with some low power IC (like TPSXXXX), but I do not want to set the output voltage to 5 V, only limit the maximum. Can anyone recommend me some IC?