Other Parts Discussed in Thread: TIDA-00778, , MOTORWARE, TIDA-00195
Datasheet section 5 Pin configuration & functions: VDD 7 ---- Bias supply input. Power supply for the input logic side of the device and also low-side driver output. "Bypass this pin to VSS with typical 1-μF SMD capacitor (typically CVDD needs to be10 × CBOOT). If shunt resistor used between COM and VSS, then also bypass this pin to COM with 1-uf (1000nf) SMD capacitor."
We use a 20mOhm ferrite in series with COM/AGND providing higher frequency VSS digital ground isolation from AGND noise. That said the COM pin is tied to AGND plane and VSS pin DGND and no shunt trace feed back path to COM pin from low side NFET. Is a 1uf bypass still required on COM pin in that case and why not place 100nf bypass on VDD pin as other gate driver vendors typically suggest? Seems odd not to have 100nf
Regarding boot cap selection (application section 8.2.2.2) suggest 0.1uf (100nf) for 87NC Qg NFET. Is it not more typical a 1uf Cboot or (100*Cg=1000nf), but not 100nf? Thus 8.2.2.3 makes second odd claim VDD bypass (10*Cboot=1uf) seemingly should be 10uf, not 1uf. Either the (not guaranteed application section) formula works for all intended purpose or leads to questions as to why did application engineer change the earlier stated rules of UCC27714 in datasheet.. Perhaps a technical Wiki could help clear up some of these application questions.
Section 9 states 22uf 50v electrolytic on VDD supply pin, why not ceramic on VDD pin as datasheet section make clear (10*Cboot value) a best practice? Very confusing contradiction to earlier stated facts of VDD bypass requirement are being made in this section. Why not say VDD source requires 22uf electrolytic. If that is not true should each UCC27714 then have a 22uf electrolytic on the VDD pin?
Section 9 Power Supply Recommendations:
The VDD power terminal for the device requires the placement of electrolytic capacitor as energy storage capacitor, because of UCC27714 is 4-A, peak-current driver. And requires the placement of low-esr noisedecoupling capacitance as directly as possible from the VDD terminal to the VSS terminal, ceramic capacitors with stable dielectric characteristics over temperature are recommended, such as X7R or better.
The recommended e-capacitor is a 22-μF, 50-V capacitor. The recommended decoupling capacitors are a 1-μF 0805-sized 50-V X7R capacitor, ideally with (but not essential) a second smaller parallel 100-nF 0603-sized 50-V X7R capacitor. Similarly, a low-esr X7R capacitance is recommended for the HB-HS power terminals which must be placed as close as possible to device pins.