Hello,
im using the UCC28051D as Inputstage to an LLC in the Powerclass of 150W. Actually I'm trying to reduce my Standby Losses. I have done a Disable Circiut, which gets a signal from the galvanic isolated secondary side to drive the VO_SNS Input into Overvoltage when disabled and releases it to normal value when enabled. So my problem no is, if I'm in disable mode the Losses of my Voltage Divider on VO_SNS and MULT_IN are about 160mW. So now i want to reduce this losses.
My Standby Power for the whole application should not exceed 0.5W.
Now my question is how low could i choose the current through this resistors? In the datasheet there are 100uA for MULT_IN Divider and 200uA for VO_SNS Divider written but in the typical application on Page 16 the current through VO_SNS is about 54uA. Is this ok or is it to low? Which drawbacks do i get with a too low current?
Thank you all for your help,
Best regards
Stefan