Other Parts Discussed in Thread: UCC28056
Hi All,
We setup the controller as calculated in the SLUC072B it will be a 600W converter.
As the unit goes above 300W the second stage is switched on. But the second switch is not switching constant at once but is going on and off with gaps. The problem is than that the input power is jumping with a difference of 50W until chanel A and B are switching constantly.
It looks like there is no hysteresis on the PHB but according to the datasheet there is.
Has anybody seen this problem and-or has a solution for this?
Thanks for the help,
Patrick