Customer has started looking at TPS65142 for the requirement of: boost Regulator 6-21V input output 9.2V (+/- 100mv) 2W.
Customer Comments:
3.3V is used to derive 9 and 28V power rails. This is 2 stage conversion with poor matching in both stages.
As we apply to notebooks: we see a 2s/3s/4s Source (6-17.8 battery) to 3.3V stage >> then 3.3V to 9V and 28V stage.
This type of topology has both a Buck and a Boost – We hold that direct conversion from Battery (2S-4S) would drop a stage completely with an additional benefit of reduced 3.3V power losses/sizing.
In the short term – a discrete path looks possible and would like to discuss a modified 65142 roadmap that would use the input power more wisely. (it already uses V_bat for example – just not this section)
Would TI propose anything different?