• Resolved

TPS65150: VGH voltage calculator

Part Number: TPS65150

HI Sir 

May I know TPS65150 can support VGH=22V when AVDD is 8.2V ? 

I saw below figure need to use AVDD 8.8V at least 

  • Hello Kai Hsiao,

    The total headroom for the double stage charge pump is mostly dependent of the diodes you are using. The output current is below 1 mA, so if you will use high-current diodes (preferably shottky) which makes sure that the voltage drop will be ~0.2-0.3 V I think you will have a good chance to get 22 V.
    But this needs to be verified on the application. Please use the equations that the application note provides.

    Best Regards.
  • In reply to Ilona:

    Hello Kai Hsiao,

    Did this answer your questions. If so please verify by clicking 'This resolves my issue'.

    Thank you.
    Best Regards.