Hi there,
well i encounter some problems regarding a TPS40210 boost converter design:
I can manage to generate 215 Vout at 24Vin using the mentioned device, but i get a heavy ripple of >2 Vpp at quite unusual low-freq. of about 28 Hz.... Actually i have no idea where this comes from... The switcher operates at about 300 kHz. The "Ripple" is even hearable as a humming sound... I tried different coils... no change...
Do you have any idea out there? Thank you!
Here is the corresponding schematic from SwitcherPro that i implemented (version 3.14.0.10):
It should be capable of delivering up to 120 mA output current dc.