Hello,
I am working on a project to drive 4 led light bars connected in series. Each light bar has typical Forward Voltage of 11.8V and Forward Current of 360mA.
I came across this web link (http://www.ti.com/lit/ml/slvr969/slvr969.pdf) showing a schematic diagram of a “40V 450mA Non-dimmable T8 LED Driver using TPS92210”.
Can the above circuitary be used to run my 4 led light bars?
If not, how do I modify the circuit to drive my 4 led light bars or is there any other equivalent circuit that I can build so that I can run my project successfully?
Best regards
Fikri