Hello,
Is it possible to control 4 strings individually with all strings connected to the Vboost?
Thanks,
Sheldon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is it possible to control 4 strings individually with all strings connected to the Vboost?
Thanks,
Sheldon
Hi Sheldon,
are you talking about case when all strings are in cluster mode?
Basic answer - yes. If current is different (I hope number of LED is same in every string), boost can be used in not adaptive mode, just to be sure voltage is enough and it is not too big to overheat chip or trigger LED shorted fault.
When part of strings are in display mode, adaptive voltage can be used - but you have to be sure this voltage is ok for cluster mode strings which are not included in adaptation loop.
EEPROM settings for fault should be chosen properly.
Best regards,
Vladimir
Thanks for the response. So I have the evaluation board for the LP8860. I have the following setup.
1. 4 strings equal LED in each string
2. Each string connected to Vboost
3. Configure EEPROM in cluster mode (setting provided in evaluation kit)
I notice that cluster 1 controls the brightness for all the LED strings, how do I configure the device to independently control each string of LEDs.
Regards,
Sheldon
Hi Sheldon,
looks like your LP8860-Q1 is not configured correctly, probably before loading EEPROM file, EEPROM is not unlocked or EEPROM is not burned.
When configuration is correct, cluster 1 controls only 1st string. Can you please disable/enable chip again and read EEPROM (Operation->Read EEPROM). Check LED driver tab, PWM mode. Should be:
Best regards,
Vladimir