Hello,
Could you please let me know the Rds(on) calculation detail?
I found that the calculation of Rds(on) from the datasheet P.11.
However this case use R(ALL)(ON)(max).Thus, this value includes Resitance of 2wire only.
For example,
If 1wire=40mohm, Rds(on)=140mohm,
Case 1 : Most upper side 1pc LED only on.
In this case, 2wire x Rds(on)*11
Case 2 : Center 1pc LED only on.
In this case, 4wire x Rds(on)*11
Thus, I think that we can’t use the calculation of the datasheet P.11 which used R(ALL)(ON)(max).
Best Regards,
Ryuji Asaka