Hi,
We are using the TPS62150 in a constant current configuration to drive a white LED up to 1A. Would like to know if there is a more efficient part.
Spec's:
Vin 2.8V-12V
Vout 3.0V @ 1A max
Thanks,
Paul
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, We looked at the TPS63060 but found the efficiency is lower than the TPS62150.
As a quick test we drove a singe LED with the TPS62150 constant voltage mode. We have not yet modified the eval board but will do soon using the recommended circuit in the data sheet and the app notes. The output current was about 800ma. at 3.3V.
I know you do not drive an LED in constant voltage mode but it was just a quick test.
Question... Driving the LED in CV mode we noticed that the input current increased considerable as the battery voltage dropped from 12V down to 5V. Can we expect the some thing to occur when we mod the eval board for CC operation?
Thanks,
Paul
Hi Chris,
I cannot believe I asked this question, of course your answer is right. Too many long hours make you forget things.
There is a question I have regarding the TPS62150. In SLVA451 it shows using this part as a single LED driver on page 2.
I understand placing a resistor on the SS/TR pin lowers the FB pin to a lower reference voltage to reduce power dissipation across Rcs.
We intend to use a D/A on the SS/TR pin with the 154K resistor. What I am not clear on is fig. 3 on page 6. If there is no voltage on this pin the current through the LED is near zero. As the voltage increases on the SS/TR pin the LED current goes up. So at system startup some voltage must be present to turn on the LED. Is this correct?
Thanks,
Paul
Hi Chris,
Referring to the schematic in the app note I did see that the graph showing the voltage applied to the SS/TR pin does show about 50ma or so of current when the pin is at 0V. That is no problem for our application.
The DAC will have no problem sinking 2.5uA. The system will be powered by a 2.0V regulator so the DAC voltage will never exceed this level. So if Vin goes to 0V so will the DAC supply voltage.
Also I noticed that the efficiency graph for analog dimming for a Vin of 4V and 17V. We plan to operate on the low end at 3V, this will be the cutoff voltage for the system, will this cause any problems with linearity?
To clarify my original question I was asking that the DAC has to have some voltage above 0V to cause a few hundred milliamps of LED current when the system is turned on.
Thanks,
Paul
Hi Chris,
That is what I thought. The high 3.6V Vf of the LED would limit the low end Vin to the switcher. We will dim the LED when the battery voltage gets near 3V. The diode as I said we are using has a lower Vf so this should give us a little more margin.
Thanks,
Paul