I bought a LP8555 evaluation board and now don't know how to use it.
1 : connection--J5,J11,J4(PIN2,3) have jump caps. I connect an external 5V to J7. LED+ is connected to boostA and LED- is connected to LEDA1,LEDA2....
2: USB virtual com port driver is installed sucessfully and the software already recgonized the connection.
3: I tried many different options but the LEDs cann't be lighted up. I measured and find there is 5V between boostA and PGND, 3V between LEDA1 and PGND. But there is no voltage between boostA and LEDA1.
4: The LED's normal working condition is 3V, 8mA. I tried single LEDs and LED strings.
The evaluation board user guide is not very clear. Is there any other guide files or could someone explain the mehod detaily? Thanks very much.