Hello,
Our customer would like to remove the Power Line FET for reducing the parts number.
When they don't use Power Line FET, the power line is not isolated from the output.
Could you please let me know the concerning point on this usage?
Also the customer use LP8861-Q1 on the following conditions without Power line FET.
If there is any concern, please let me know.
Vin=8.7V, Vboost=22V, Iled=40mA x 4string =160mA, Fsw=2.2MHz
Cin=10uF cer. x 3pcs, Cout=10uF cer. x 3pcs
Best Regards,
Ryuji Asaka