Hi.
I have a question while reviewing the TPS61196-Q1.
"Each string has An independent current regulator providing a LED Current adjustable from 50mA to 400mA within ± 1.5% matching accuracy ".
However, we will use 20mA per CH.
I want to know if it is supportable.
1. The operating voltage is 12V INPUT
2. The output voltage is Max 78.2V
3. Current per Ch is 20mA
Can you confirm that the TPS61196-Q1 product meets the above conditions?