Hello,
I have a problem with the LP8860.
Sometimes the circuit with the LP8860 provides a short circuit for the voltage supply immediately after switching on.
The voltage then breaks from 24VDC to about 3VDC.
Often, the fault has disappeared again after a new voltage is switched on, so the LP8860 works properly.
Now I have the problem that the LP8860 permanently forms a short circuit between Vdd and ground (the connection Vdd to the rest of the circuit is separated).
Obviously the chip is defective.
How can the problem occur and how can I prevent it in the future?
Thank you
Dieter