Other Parts Discussed in Thread: TPS92515
Team,
I have a customer who is using TPS92515 in their application (previous post here: ) that is wondering the following: what is the minimum overhead the part needs to be stable? If they are attempting to drive a 22V OLED, they are reporting that it requires around 24V for the part to remain stable. They were hoping to get this value down to 23V. Is this a factor that is inherent to the part (and if so, what is the value?), or is this something that can be tweaked via circuit?