1. I have to control a 3W single led intensity, need to vary intensity linearly from 0 to 100% as user rotates potentioneter of 10K.
2. is there any dedicated low cost asic solution available for this, which can do this.
3. Most of i have checked need a PWM signal to ic like here
www.ti.com/.../products.html Linear;DC/DC&p2297=Analog
I am looking for some solution where a potentiometer can do the dimming directly, instead of connecting additional ckt for asic
4. Voltage of Li-Ion cell: 3 to 4.2V
if charging, then voltage go to 5V from main adapter
So input voltage for IC go from 3V to 4.2V