Hi all,
few simple questions:
1)after dialing in data and latching it into the output, can the CLK signal be removed without disrupting output ?
2)if so, is it better to set CLK HI or LO or doesnt matter?
3)By using the special mode to reduce the control voltage, is it possible to reliable dim outputs to 1/12 of the min current of 5 mA ? Or would 5 mA still be the min reliable current?
Thanks in advance,
Tobias