I´m using a TLC5944 for a project where I want drive 16 RGB LEDs but I have a problem with ghosting.
Each LED cathode are directly connected to the TLC outputs.
To drive each column of anodes (RGB) I tried two solutions:
The first was with a TC4469 and all works fine but this driver only can deliver 250ma and is not sufficient when I want turn on all 16 LEDs at the same time.
My second choice was try a "totem pole" configuration as I saw on the datasheet, everything seemed to be fine and all 16 LEDs turn on at same time, but the ghosting problems began here when I saw the red emitter with a little glow.
The problem is present with a VLed = 5V and if Vled = 12V also the green emitter show the same problem.
I tried with two different models of MOSFET to build the "totem pole" high-side (IRF7105, IRLML6402 and complementary) and the problem is the same. I tried changing the Rgate for reduce ringing and the problem is minor but all leds are dimmed.
For multiplexing I'm working with a low frequency (1.63KHz) and each duty cycle for RGB is 1/3 from 1.63KHz.
How I say before, if I use TC4469 the ghosting problems disappear. I can't understand what is wrong with my totem pole.
Several days ago I'm trying to solve this problem but I can't.
Could somebody help me please? May be a suggestion or send me a schematic for build the right driver, please
Thank you
Julio