Hello,
I have a problem that I can not find solution. I used the LDO's TPS7A4901 and the TPS7A3001 regulators to make a complementary power supply. The schematic and the PCB are the same for both LDO. Are the typical datasheet schematic :
The negative part with TPS7A3001 work successfully with zero problem, but the positive part with TPS7A4901 work for maximum 5/10 minutes whit an unstable output range (12 to 14 Volt) and after it destroys!! I have solderet five PCB's and i tried to change the ratio resitances (R1= 470K R2=47K), but all give roughly the same problem!!!
Could you help me to solve the problem? thing is that it changes from a negative to a positive LDO? What changes from a negative to a positive LDO?
thank you
Alessio