This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help me!! Big Problem with TPS7A49xx

Other Parts Discussed in Thread: TPS7A49, TPS7A30

Hello,

I have a problem that I can not find solution. I used the LDO's TPS7A4901 and the TPS7A3001 regulators to make a complementary power supply. The schematic and the PCB are the same for both LDO. Are the typical datasheet schematic :

 

The negative part with TPS7A3001  work successfully with zero problem, but the positive part  with TPS7A4901   work for maximum 5/10 minutes whit an unstable output range (12 to 14 Volt) and after  it destroys!! I have solderet five PCB's and i tried to change the ratio resitances (R1= 470K R2=47K), but all give roughly the same problem!!!

Could you help me to solve the problem? thing is that it changes from a negative to a positive LDO? What changes from a negative to a positive LDO?

thank you

 

Alessio