Hello. I'm trying to figure out why my Bad Thing(tm) meter is going off, and I can't quite put my finger on it.
We have a situation with a proprietary open-collector low frequency bus. A number of devices may have their logic inputs connected to ("reading") this bus with 10K (or greater) pullups to the device's supply rails. Some of the devices operate at 12V and some at 5V. Basic assumption that both rail voltages are being generated by 78xx type LDO regulators. Some of the devices are in-house design, but some are third-party legacy gear that we will have to accommodate.
So far, best I can figure is that since the LDO outputs are connected through two 10K (min) series resistors, the actual bus voltage will be halfway between the supply voltages (~ 7.5V assuming a 7812 and a 7805), and there will be a small current (~ 0.35mA) flowing from the 12V through the pullups into the 5V circuit load, reducing the load slightly on the 5V regulator and increasing the load on the 12V regulator. I want to think that the resistors between the outputs will allow the two regulators to operate independently, but something tells me I am missing something.
I've read plenty about how it is a bad thing to directly tie the two different LDOs outputs together, but is it also bad to allow this path through the pullups?
Thank you!
- Mark Underwood