The datasheet for the TPS7A4101 requires at least a 1uF cap on the input for stability. However, Figure 13 (see below) in the datasheet does not show an input capacitor. When the device is used for driving LEDs with a PWM signal connected to the EN pin, is an input capacitor required? What is the range of the switching frequency allowed on the EN pin?