I just want to use TPS7A8101 LDO to get a output voltage 3.3V. I do the design according to the datasheet. But the problem is that now the output voltage is same as input voltage. Eg, input voltage is 3v, then output voltage is 3v too, Or input voltage is 5V and the output voltage is 5V as well. It looks FB doesn't work. I measure the NR pin, the voltage is fixed at about 0.8V, but the FB pin's voltage is not fixed, it looks changed with the output voltage. But in theory, the FB pin's voltage should be fixed and output voltage should be fixed too if the divider resistors determined.
Can anybody help me on that, I am very confused now.
Thanks in advance.