Hi,
I have sensor that can operate between 1.9V and 3.6V, but likes 3V. The sensor will be using a 4.7V LiPo and a 6V PV panel. I am looking of either an LDO or Buck Boost regulator that can regulate a voltage, but if the voltage goes below the regulated amount the regulator will allow the sensor to still be powered on a lower voltage. Or, may be if can just regular the voltage between 1.9V and 3.3V, and shut off below 1.9V. The sensor needs no more the 100mA to operate.
Any advice/help would be greatly appreciated.
Best,
Stephen.