客户目前用的型号是TLV70433,由于输出最大是150mA, 而且负载的峰值电流已经达到150mA,所以客户需要留出一定的余量,
目前客户的要求是:输入3.3v-12v,输出3.3v,200mA
找到TLV70033可以封装兼容,但是输入电压最大是5.5V,不满足要求,
请帮忙推荐个合适的型号
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
客户目前用的型号是TLV70433,由于输出最大是150mA, 而且负载的峰值电流已经达到150mA,所以客户需要留出一定的余量,
目前客户的要求是:输入3.3v-12v,输出3.3v,200mA
找到TLV70033可以封装兼容,但是输入电压最大是5.5V,不满足要求,
请帮忙推荐个合适的型号
Hi Iaisan,
The closest match for low-Iq, wide-Vin, and >150mA output current is the TPS7A19.
Regards,
David