Hello,
Are there any plan to release the LDO which have following specification?
Vin range : 3.0V to 4.2V
Vout :105V ± 0.1V
Output current : 350mA(max)
Output Discharge
Internal Pull Down in the EN pin
Size : about 0.8mm×12.mm×0.5mm
I think that the TPS7A91 is similar to this requirement.
Best Regards,
Ryuji Asaka