Hi all
Would you mind if we ask TPS737?
<Question1>
Do you have VFB(Internal reference) data with Tj=-40 to 125C?
The data sheet shows in case of Tj=25C.
So, there is the description "Over operating temperature range (TJ = –40°C to 125°C)", so do Min and Max value mean in case of Tj=-40 to 125C?
<Question2>
Is there internal(weak) pull-down resistance at EN pin?
If there is internal pull-down resistance at EN pin, how much is the tolerance?Approx ±20%?
<Question3>
When Vin < Vout occurs, will the device be damaged?
We guess that there are follows cases;
-Case1 : Vout asserted transient voltage(or surge) -> as the result, Vin < Vout
-Case2 : Discharge time difference between Vin and Vout -> as the result, Vin < Vout
-Case3 : Vin is abnormal(short) -> as the result, Vin < Vout
At all cases, we concider that the device will be damaged, right?
<Question4>
In relation to <Question3>, according to insert diode between Vin and Vout, is it possible to prevent from damage?
If we insert the diode Vin and Vout, should we be concerned about ocillation(stablity)?
<Question5>
If you have the data of phase margin and gain margin using EVM(TPS73701DRVEVM-529), could you give us as reference(including Vin, Vout/Iout condtion)?
Of cource, we recognize that gain margin is enough(at least more than 60 degree).
<Question6>
About CFB, how much is the time constant which is limit of response?
Usually, we should use CFB less than 0.1uF.(On the datasheet, there is the description 10nF.)
We appreciate your help always.
Kind regards,
Hirotaka Matsumoto