Hi All,
I am using the TPS40210 in a boost app that takes a 12V battery supply and generates 30V at 2.5A to run a motor.
For the output cap, it will have to abosrb some energy dumping from the motor when the motor returns energy to the power supply and the output cap also has to handle the AC component from the boost topology.
Question :
- Is the ESR for the output cap in the example calculation a maximum amount or a target ESR that is required. Can I just use caps in parallel to increase the ripple current rating and also to lower the ESR.
- This is probably a really newbie question but what is the AC current that the caps have to handle. Is it equal to the worst case ripple current in the inductor?
cheers
Peter