Hello,
I'm using the TPS61040 chip.Specifically, the 3.3V to 12V reference circuit that is in Figure 20. I'm using the recommended inductor and diode, as well as the same values for the capacitors. Resistor values are slightly different. I've implemented this on a custom board.
Unfortunately, I'm getting some strange waveforms, and some ripples/spikes on the input (3.3V) power line as well as the output (12V) power line. These waveforms were collected with a load of 300 ohms. I've attached these waveforms below.
Any idea what might be going on? How can I reduce these spikes and ripples on both the input and the output?
Switching voltage
Input
Output