Hi,
We have a board that uses LM2841x buck regulator IC to derive 3.3V, 100mA output (IC load) from (4.5V - 40V) input range. We are seeing a lots of failure in the field.
While investigating, we saw that the IC fails when the input power is turned on sharply from 0V to 30V (in ~20-30 usec). Some times the failure occurs after switching the input on multiple times at this rate and sometimes it gets reproduced at low temperature (-25degC and below) at lower input voltage.
Anybody has faced this issue? What might be the reason? Any solutions?
Regards,
Sanjib