Hello,
I have built a regulator based on LM5116
Vin from 24 to 80 V. Vout is 15 V. Iout is 2 A.
No load is connected initially.
The regulator works well when Vin is from 24 to 40 V. But, when I ramp more than 40 V, the LM5116 gets heated up and stops working (Vout = 4.6V).
I have built the circuit using TI Webench on a general purpose PCB. So the layout is not to the mark as per the datasheet.
Attaching the Webench design file.
Waiting for your kind reply.