I purchased a TPS65251EVM eval board for verification of this part for a new design, but I’m not measuring efficiencies anywhere near what’s show in the TPS65251 datasheet.
For example, buck 3 of the EVM is setup for 3.3V output and the datasheet shows in fig 17 that the efficiency should be about 95% for output currents of 0.2 – 0.3A yet I measure efficiencies in the range of 87% to 91%.
Buck 1 is setup for 1.2V and fig 6 shows an efficiency of 88 – 90% for currents of 0.2 – 0.3A but I measure efficiencies of 71 – 76%.
How were the efficiency plots in the TPS65251 datasheet measured?
The eval board draws about 27mA @ 5V with all 3 switchers enabled but no loads, so how can this part provide the low-current (0.1 – 0.2A) efficiencies shown in the datasheet?
Is there a better part to look at for higher efficiencies for 3.3V, 2.5V and 1.2V outputs from 5V for output currents in the range of 0.2 – 0.4A?
Thanks,
Steve