Hi
I Want to use TPS40210 for some boost power supply. I got a boost converter designed using SwitcherPro & device TPS40210 for 13-11V to 48V @ 1A boost converter. The out put is not boosted but input - diode drop. On checking The frequency at RC pin (1) is found to be about 480Khz and Voltage at BP pin (9) is 8.13 V but no voltage at GDRV pin (8).
1. Can open PWRPAD cause this?
2. what more to be checked to ensure the units proper functionality.
3. When I make the feed back zero my output voltage increase to 15 Volt
4. Then the diode shown in the schematic is BAT 46W which I believe is not suitable. I dont understand how the the SwitcherPro suggested it.
I am confused please help.
Regards, Sunil