The customer would like to know if the thermal pad on the TPS61170DRVT is internally connected to ground or not as he will be having a negative voltage on ground.
-12V to -5V converter: (See attached file: 12VN_5VN converter.PNG)
This uses the TPS61170. Here we are really unsure about the requirements for the GND-EP (thermal pad). We initially had this connected to earth ground, but as with the other part we now wonder if it should be connected to the same potential as pin 3 (GND).
Any information on the internal electrical connection of the thermal pads for these parts is greatly appreciated.