Hello
I have a question.I would like you to tell me.
written in the datasheet, Ton-time=Vout/Vin*400ns .But TOFF time not written.
When I measured at TPS62130EVM. TOFF= about 130ns.
The actual value some?
Regards
T Kishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have a question.I would like you to tell me.
written in the datasheet, Ton-time=Vout/Vin*400ns .But TOFF time not written.
When I measured at TPS62130EVM. TOFF= about 130ns.
The actual value some?
Regards
T Kishi
Thank you for clarifying. Yes, the frequency in figure 19 decreases for 2 reasons: higher drop across the high side MOSFET and a minimum off time. At lower Vins, the Rdson increases a little bit, so the on time must be extended to overcome these losses. This will decrease the frequency since the on time must be longer than expected.
At higher duty cycles, you will see a ~130 nsec minimum off time which also decreases the frequency for very high duty cycles.
The output remains regulated in both cases and there is no issue operating in this region. Using the 1.25 MHz frequency setting will make the variation from the minimum off time have a smaller effect on the frequency.
Is this an issue in your application? What power specs do you need to meet?
Hi Chris
Thank you for reply.
I want to one question.
Change the FB resistance(R1) of TPS62130EVM, Vin=3.3V, Vout=2.0V, Duty=60%, Iout=500mA, SW=2.5MHz
If this condition,PWM mode should operate at 2.5MHz.
But check the waveform,SW=about 1.5MHz
ON time=480ns,OFF time=240ns (fix)
I want you to tell me why this happens
Regurds
T kishi
Hi Chris
I want to point out me, if i think is different.
I think Off time is Fixed,When around 6Vin.And Off time is diffrent by Vout.
ex)Vin=6.0V Vout=1.26V Off time=about 120ns
Vin=6.0V Vout=2.0V Off time=about 220ns
I was measured ins this condition.
Vin=4.0V Vou=1.26V Off time=about 120ns
Vin=4.0V Vou=2.0V Off time=about 220ns
Therefor,Frequency begin around 6Vin,Off time of when the diffrent by Vout.
if match my guess is,the problem become clear.
Regurds
T kishi
Hi Chris
This problem,described my customer.
So ther is a request,Do you have any infomation such as Application notes or Documents on this issue?
I would like to have if there is material.If not ,to negotiate to my customer.
Best Regurds
T Kishi