Hi,
I'm considering to use Buck-boost DCDC converter by TPS63061.
The condition is as follows.
Input voltage : 4~7V
output voltage : 5V
load current : 100mA(Typ) / 500mA(Max)
The PS/SYNC pin is connected to GND directly by PCB wire.
A load current is little and it's driving in PFM mode , and the output voltage is 5.15V.
At first, the range of output voltage in PFM mode.
In the datasheet, threshold voltage are 2.5% and 3.5% at typical condition.
But , it's not written at worst condition.
I would like to know the threshold voltage of ripple at PFM mode.
I'd like to improve the output voltage precision, so I'd like to make them drive by a PWM mode.
But, it's impossible to re-connect the PS/SYNC pin to VIN.
Is it possible TPS63061 operate in PWM mode or like a PWM mode while the PS/SYNC pin isconnected to GND?
I'd like to know that if there is a way .
Thanks.