Hi,
I guess that the equation (51) in the D/S is wrong.
Firstly, when the equation (48) in the D/S is changed, it becomes "GMOD(fc)*gm(EA)*Rc=Vout/Vref".
I'm thinking that this equation is to calculate Rc as the modulator voltage gain x the error amp voltage gain = Vout/ VREF.
And, I'm thinking the units the left-hand side and right-hand side are [V/V].
On the other side,
when the equation (51) in the D/S is changed, it becomes "GMOD(fc)*gm(EA)*Rc*fz(mod)=Vout/Vref".
I cannot understand multiplying "fz(mod)".
And, I'm thinking the unit of the left-hand side is [Hz*V/V], right-hand side is [V/V].
I think that this is and error.
And, when I check the D/S of TPS54260, a equation calculating RC is only 1(it isn't divided Low ESR and high ESR).
So, I think that the equation is wrong.
Could you advise me ?
Thanks and Regards,
Kuramochi