I bought an evaluation board "SV600184-001 LM3481SEPICEVAL/NOPB", and I did tests with the cispr22 and the result was bad, 80MHZ, I did a PCB with the same mode and did the same problem with EMI, what can I do to solve it? My application is a DCDC converter with 3 outputs, 18Vx1A, -18Vx1A, 5Vx1A, the input 26V.
Airton.