In TPS53355 datasheet (SLUSAE5B), it is written that EN pin turn-on threshold is 1.2V and turn-off threshold is 0.95V on P.3. However EN voltage min value is 1.8V and Disable voltage max value is 0.6V on P.6.
I think this is the datasheet misdescription on P.6, then my idea is the following, is this correct?
1.2V and 0.95V is typ value
1.8V is Enable max value
0.6V is Disable min value.
Best Regards,
Kohei Sasaki